The E4982A display screen include the six types of displays (two measurement displays and four setup displays) as explained in the table below:
|
Display type |
Function |
|
|
Measurement display |
Measurement is done at the specified single measurement point and the result is shown on this display. |
|
|
All measurements are preset in the specified table according to the sequence of the measurement point numbers and are listed on the display. Plotting mode is available. |
||
|
Setup display |
A display for setting up measurement points. The required measurement points are set sequentially, starting from measurement point number 1, by inputting measurement conditions (measurement frequency, averaging factor and test signal level). A maximum of 201 measurement points can be set in each of the eight tables. |
|
|
A display for setting up the calibration kit definition (value) for the measurement point set up on the measurement point setup display. |
||
|
A display for setting up the compensation kit definition (value) for the measurement point set up on the measurement point setup display. |
||
|
A display for setting up the conditions for bin sorting (sorting by measurement result). |
||