External and auxiliary triggering is used to synchronize the triggering of the analyzer with other equipment.
How to make Trigger Settings:
A 'Ready for Trigger' signal is different from a Trigger signal. The ready signal indicates that the instrument sending the signal is ready for measurement. The instrument receiving the ready signal would then send a trigger signal, indicating that the measurement will be, or has been, made. Usually the slower instrument sends the trigger signal.
Learn more about each type of triggering signal:
Meas Trig RDY and Meas Trig IN - This pair of signals is easy to use and limited in ability to configure.
AUX TRIG - The connectors and signals are highly configurable. Use them to synchronize with any number of devices and equipment.
Meas Trig RDY and Meas Trig INThe MEAS TRIG connectors are located on the rear-panel. These signals can be used when the analyzer is communicating with a slow mechanical device. A material handler is very mechanical and takes a relatively long time to load and discharge parts. Here is how these signals work together to communicate:
See how to access the Trigger Dialog Dialog SettingsTo cause the SSA to respond to Meas Trig IN or Handler I/O signals, select External on the Trigger Setup tab, Source setting. Note: You must select External when you use any external triggers. Also on the Trigger Setup tab, Scope setting, choose whether one external trigger signal will apply to ALL channels (Global) or one trigger signal per Channel. The following settings apply accordingly. Main Trigger Input Global / Channel Trigger Delay After an external trigger is received, the start of the sweep is held off for this specified amount of time plus any inherent latency.
Source The analyzer accepts Trigger IN signals through the following connectors:
Level / Edge High Level The analyzer is triggered when it is armed (ready for trigger) and the TTL signal at the select input is HIGH. Low Level The analyzer is triggered when it is armed (ready for trigger) and the TTL signal at the select input is LOW. Positive Edge After the analyzer arms, it will trigger on the next positive edge. If Accept Trigger Before Armed is set, the analyzer will trigger as soon as it arms if a positive edge was received since the last data was taken. Negative Edge After the analyzer arms, it will trigger on the next negative edge. If Accept Trigger Before Armed is set, the analyzer will trigger as soon as it arms if a negative edge was received since the last data was taken. Accept Trigger Before Armed When checked, as the analyzer becomes armed (ready to be triggered), the analyzer will immediately trigger if any triggers were received since the last taking of data. The analyzer remembers only one trigger signal. All others are ignored.
Ready for Trigger Indicator (Trigger Ready)On the analyzer, when External is selected on the Trigger Setup tab, then both Meas Trig IN and Meas Trig Ready are enabled. Note: The Ready for trigger is available only when the trigger source is set at External. Choose a connector to send the analyzer Ready OUT signal: Choose Polarity of the 'Ready OUT' signal.
See Also |
See how to access the Trigger Dialog AUX TRIG OUT and AUX TRIG INNote: AUX Trigger IN and OUT are supported only in Network Analyzer (Standard) and Spectrum Analyzer measurement classes. The other measurement classes do not support them. These signals are highly configurable. They can be used with all types of external devices to send and receive signals. However, it is important to note that either Aux Trig INPUT does NOT trigger the VNA. That signal must be selected. See step 2 in the following procedure.
Dialog SettingsThe Aux Trig 1 tabs are identical. Two pair of connectors are available to allow two external devices to be controlled simultaneously. Enable Check to use the Aux connectors to output signals to an external device. Channel: This setting is controlled by a Preference setting.
AUX TRIG OUT (To Device)The following settings control the properties of the signals sent out to the AUX connector. Polarity Positive Pulse Outgoing pulse is positive. Negative Pulse Outgoing pulse is negative. Position Before Acquisition Pulse is sent immediately before data acquisition begins. After Acquisition Pulse is sent immediately after data acquisition is complete. Per Point Check to cause a trigger output to be sent for each data point. Clear to send a trigger output for each sweep. When the Aux Trig - "Global" Preference is selected, then the Point setting is made on the Trigger Setup tab. It then applies to ALL channels. When more than one channel is present, the channel setting that was made last is used. Pulse Duration Specifies the duration of the positive or negative output trigger pulse. Enable Wait-for-Device HandshakeWhen checked, the analyzer waits indefinitely for the input line at the application IO (pin 7) to change to the specified level before acquiring data. This signal indicates that the external device is ready for analyzer data acquisition. If the signal arrives before the analyzer is ready to acquire data, it is latched (remembered). When NOT checked, the analyzer does not wait, but outputs trigger signals when the SSA is ready. This signal does NOT trigger the analyzer. The trigger signal is generated from Trigger Sources: Internal, Manual, or External. IN (READY) Positive Edge The analyzer responds to the leading edge of a pulse on the Aux1 or Aux2 In connector. Negative Edge The analyzer responds to the trailing edge of a pulse on the Aux1 or Aux2 In connector. Delay Time that the analyzer waits after receiving the Handshake input before data acquisition begins. See Also
|