A sweep is a series of consecutive data point measurements taken over a specified sequence of stimulus values. You can make the following sweep settings:
Number of Points (Separate topic)
Frequency Range: Start/Stop (Separate topic)
See Triggering and other 'Setup Measurements' topics
How to set Sweep Type |
|
Using Hardkey/SoftTab/Softkey |
Using a mouse |
|
|
Note: Sweep Settings are not applied until either OK or Apply is pressed. Channel The active channel when Sweep Type was selected. Sweep settings will be applied to this channel. Sweep TypeLinear Frequency Sets a linear frequency sweep that is displayed on a standard grid with ten equal horizontal divisions.
Log Frequency The source is stepped in logarithmic increments and the data is displayed on a logarithmic x-axis. This is usually slower than a continuous sweep with the same number of points.
Power Sweep Activates a power sweep at a single frequency that you specify. Learn about power sweep
CW Time Sets the analyzer to a single frequency, and the data is displayed versus time. Learn more.
Segment Sweep Sets the analyzer to sweep through user-defined sweep segments. Learn how to make these settings.
OK Applies setting changes and closes the dialog box. Apply Applies setting changes and leaves the dialog box open to make more setting changes. Cancel
Closes the dialog. Setting changes that have been made since
the last Apply button click are NOT applied.
|
|
A power sweep either increases or decreases source power in discrete steps. Power sweep is used to characterize power-sensitive circuits, with measurements such as gain compression.
In the Sweep Type dialog, specify Start power, Stop power, and CW Frequency. Power can be swept over any attainable range within the analyzer ALC range.
The remaining power settings apply in power sweep mode:
Test Port Power setting is not available.
Port Power can be coupled or uncoupled.
Attenuator Control is always Manual.
Power Slope (dB/GHz) is ignored (output frequency is CW).
Press Sweep > Main > Number of Points to change the step size of the power sweep.
Notes:
Using a preference setting, you can specify whether to maintain source power at either the start power or stop power level at the end of a power sweep.
Power Sweep is optimized for speed. For highest measurement accuracy during a power sweep, it may be necessary to increase the Dwell Time to allow the source more time to settle.
Segment Sweep activates a sweep which consists of frequency sub-sweeps, called segments. For each segment you can define independent power levels, IF bandwidth, and sweep time.
Once a measurement calibration is performed on the entire sweep or across all segments, you can make calibrated measurements for one or more segments.
In segment sweep type, the analyzer does the following:
Sorts all the defined segments in order of increasing frequency
Measures each point
Displays a single trace that is a composite of all data taken
Restrictions for segment sweep:
The frequency range of a segment is not allowed to overlap the frequency range of any other segment.
Note: Segment sweeps can be overlapped for converter measurement types.
The number of segments is limited only by the combined number of data points per channel (1 to 100,003 points) for all segments in a sweep.
The combined number of data points for all segments in a sweep cannot exceed the max number of data points per trace.
Segment Table Softkeys Add Segment - adds a sweep segment at last segment. Insert Segment - adds a sweep segment before the selected segment. You can also click the "down" arrow on your keyboard to quickly add many segments. Delete Segment - removes the selected segment. Delete All Segments - removes all segments. Note: At least ONE segment must be ON or Sweep Type is automatically set to Linear.
Segment Table dialog box X-Axis Point Spacing - Check to scale the X-axis to include only the segments. Learn more. Allow Arbitrary Segments - Check to allow arbitrary frequencies (overlapped or reverse sweep). Learn more. Display Center/Span Freq - Check to display the center/span frequency.
Independent Setting Per Segment Power Level - Sets the Power level for the segment. Also, the test port power can UNCOUPLE. See Power Coupling. IF Bandwidth - Sets the IF Bandwidth for the segment. IF Bandwidth Per Port - Sets the different bandwidth with different port for the segment. Sweep Time - Sets the Sweep time for the segment. Dwell Time - Specifies the time the source stays at each measurement point before the analyzer takes the data. Vector Averaging - Enables SA vector average for the segment. Video Bandwidth - Enables SA video bandwidth for the segment. Delay- Sets the time to wait just before acquisition begins for each segment. Sweep Mode - Sets the sweep mode to auto or stepped. Shift LO- Sets the state of Shift LO. Receiver Atten Per Port - Enables receiver attenuation per port for the segment. Receiver Gain - Sets Receiver Gain. Reference Tone - Enables SA multitone reference for the segment. SA Data Threshold - Enables SA data threshold for the segment.
Save Table - Saves the setting changes in segment table. Load Table - Apply the setting changes in segment table.
To Modify an Existing Segment To make the following menu settings available, the segment table must be displayed first. (Press Sweep > Segment Table). State - Click the box on the segment to be modified. Then, use the up/down arrow to turn the segment ON or OFF. Start - Sets start frequency for the segment. Click the box and type a value and the first letter of a suffix (KHz, Mhz, GHz). Or double-click the box to select a value. Stop - Sets stop frequency for the segment. Click the box and type a value and the first letter of a suffix (KHz, Mhz, GHz). Or double-click the box to select a value. Note: The segment table truncates the frequency resolution. To verify the frequency resolution that you input, create a marker at the start or stop frequency settings. Points - Sets number of data points for this segment. Insert a value or double-click the box to select a value. To set Power Level, IF Bandwidth/IF Bandwidth Per Port, Sweep Time, Delay, Receiver Attenuator Per Port, Sweep Mode and Shift LO independently for each segment:
Note: If the following are NOT set, the entire sweep uses the channel IFBW, Power, and Time settings. |
This feature affects how a segment trace is drawn on the screen.
How to select X-Axis Point Spacing |
|
Using Hardkey/SoftTab/Softkey |
Using a mouse |
|
|
Without X-axis point spacing, a multi-segment sweep trace can sometimes result in squeezing many measurement points into a narrow portion of the x-axis.
With X-axis point spacing, the x-axis position of each point is chosen so that all measurement points are evenly spaced along the x-axis.
For example, given the following two segments:


Without X-Axis Point Spacing

With X-Axis Point Spacing
This feature allows arbitrary frequencies to be entered into the segment sweep table. With this capability, segments can have:
overlapping frequencies.
the stop frequency less than the start frequency (reverse sweep).
However, there are several limitation:
Sweep mode: Stepped only.
Sweep time: When reverse sweep is performed, the sweep time and the wait time before the measurement point becomes longer.
How to enable Arbitrary Segment Sweep |
|
Using Hardkey/SoftTab/Softkey |
Using a mouse |
|
|
Notes:
Unusual results may occur when using arbitrary sweep segments with markers, display settings, limit lines, formatting, and some calibration features.
When Allow Arbitrary Segments is checked, a dialog is displayed indicating that X-axis point spacing is recommended.
When the segment table has both forward and reverse frequency sweep, the correction interpolation may not work properly. Use the same segment table setting for both correction and measurement. (Make a measurement at the condition where "Cor" is displayed.)
When the measurement data size of segment table exceeds its limitation, an error occurs. In this case, reduce the measurement data size (i.e., NOP, number of channels).
The analyzer automatically maintains the fastest sweep time possible with the selected measurement settings. However, you can increase the sweep time to perform a slower sweep.
How to set Sweep Time |
|
Using Hardkey/SoftTab/Softkey |
Using a mouse |
|
|
Sweep Time Specifies the time the analyzer takes to acquire RF data for a sweep. The maximum sweep time of the analyzer is 86400 seconds or 1 day. Learn about other settings that affect sweep speed. Note: When a channel has an Aux In or SMU trace, the measurement time for DC voltage/current will be added. |
|
How to make Sweep Setup settings |
|
Using Hardkey/SoftTab/Softkey |
Using a mouse |
|
|
TimeSweep Time - same as Sweep Time Softtab Help. Dwell Time - Specifies the time the source stays at each measurement point before the analyzer takes the data. See also Electrically Long Devices. Sweep Delay - Specifies the time to wait just before acquisition begins for each sweep. This delay is in addition to Dwell Time (per point) and External Trigger delay if enabled. Sweep ModeAuto - Automatic adjusts the sweep time and dwell time. When "Auto Sweep Time" is checked, the sweep time and dwell time will disable to edit. Stepped When checked (Stepped Sweep) the analyzer source is tuned, then waits the specified Dwell time, then takes response data, then tunes the source to the next frequency point. This is slower than Analog Sweep, but is more accurate when testing electrically-long devices. When cleared (Analog Sweep) the analyzer takes response data AS the source is sweeping. The sweep time is faster than Stepped, but could cause measurement errors when testing electrically-long devices. When the dialog check box is cleared, the analyzer could be in either Analog or Step mode. The mode can change from sweep to sweep. There is NO way to determine whether the analyzer is in Analog or Stepped Sweep. If you want to be sure what the current sweep mode is, then switch it to Stepped. Stepped sweep is automatically selected for a number of reasons. Here are some of the reasons:
|
|