Other topics about Revision History
The revision B.xx.xx is for the E5061B with Windows 7/10. The revision A.xx.xx is for the E5061B with Windows XP.
Support Windows 10
Straight Limit Line in Log Sweep (Line Spacing in Limit Test)
Add the five commands to change the manufacturing name and model number.
SYSTem:PERSona:xxxx
Option 3L4/3L3 is supported.
Option 006 Wireless Power Transfer Analysis is supported.
Overload Detection function is enhanced.
Keysight Rebranding
Firmware update procedure is changed.
Network setup menu is changed.
Supports Windows 7
Bug Fix
Bug Fix
Segment Sweep: IFBW Auto function does not work in the Segment Table even if IFBW AUTO is ON.
Initial Source Port Control function: The DC bias and RF/LF source can be set on/off independently.
Overload Recovery: Clear Overload Protection function is added. The measurement is aborted when overload is detected.
SCPI.SYSTem.ISPControl.STAT: This commands turn on/off the initial source port contron for RF signal only.
The following commands have been added:
The first revision of E5061B firmware. This revision is for DEMO unit only.