Last Updated: August 29, 2007
This topic lists all of the available SCPI commands in the E6832A W-CDMA Cal Application.
It is recommended that you print this topic because it provides a useful syntax reference for all of the available W-CDMA Cal Application commands. To print:
Click the Print icon on the toolbar above, or
Right-click in this topic pane and select Print...
The SCPI commands in this topic are categorized by subsystem: