For security reasons, you can prevent frequency information from appearing on the VNA screen and printouts.
How to set Frequency Blanking |
|
Using Hardkey/SoftTab/Softkey |
|
|
|

Security Levels None - All frequency information is displayed. Low - No frequency information is displayed. Return to this dialog box to re-enable display of frequencies. Frequency information is blanked from the following:
Note: Frequency Blanking is fully supported ONLY on Keysight MXG sources with option 006. On MXG models without option 006 and all PSG models, the window state is turned OFF. When the “local” button is clicked on the source, then frequency is re-displayed. High - No frequency information is displayed. Only Preset or recall of instrument state can re-enable display of frequencies. Low security level settings PLUS:
Extra - Frequency information is not displayed and will not be saved to ASCII file types. Only Preset or recall of instrument state can re-enable display of frequencies. High security level settings PLUS:
For ALL security levels:` Frequency information is NOT blanked from the following:
Instrument State and Cal Sets The security level is always saved and recalled with an instrument state. However, the instrument state may contain a Cal Set or link to a Cal Set. Learn more. This may influence the security level when the instrument state is recalled.
|
Last Modified:
|
18-May-2016 |
First Release |