If make an incorrect setting, you can quickly recover by selecting Undo. If Undo incorrectly a setting, you can Redo the undone setting.
Undo and Redo applies ONLY to selected VNA settings.
The Undo stack remembers 16 levels of Undo-able settings.
Tips:
|
|
|
|
Undo |
Redo |
Undo/Redo can be stored to a User Key or Favorite softkey.
With a keyboard:
Undo --> Ctrl+Z
Redo --> Ctrl+Y
To clear the Undo stack, press Undo > Main > Clear Undo History.
Undo/Redo is disabled with High and Extra security levels. Learn more.
State files that are saved for Undo/Redo purposes (for example: Preset) are deleted when any of the following occur:
The VNA Security level is changed
The VNA App is started or closed.
You can Undo or Redo the following VNA settings:
Note: There are several VNA settings that are NOT Undo-able. Because of this, when you attempt to Undo a long sequence of operations, it is unlikely that the original state can be recreated exactly.
For Standard Class: Start, Stop, Center, Span, CW
For SMC: Mixer Setup dialog Apply
Power Level - most applications and S-parameters
Window Tile
Move Trace, Drag Trace
Measurement Setups dialog
Single Marker Searches (Max, Min, Target, Peak…)
Multi-marker Searches (Bandwidth, Power Saturation, Normal Operating Pt)
Change a Marker’s stimulus value: softkeys, dialog or drag
Change cell in Segment Table
Mechanical Settings dialog
Last modified:
|
18-May-2016 |
First Release |