The Signal Studio for Mobile WiMAX advanced carrier mode supports testing of the STC/MIMO features needed for Wave 2 of the WiMAX Forum’s Radio Conformance Test, including:
Space-Time Coding (STC): Transmit diversity is supported to provide spatial diversity and reduce fade margin
Spatial Multiplexing (SM, also known as MIMO): With spatial multiplexing, multiple streams are transmitted over multiple antennas. With 2x2 MIMO, SM increases the peak data rate two-fold by transmitting two data streams. Two data stream multiplexing method are addressed in 802.16e-2005: horizontal encoding and vertical encoding. Only vertical encoding is supported in the Signal Studio for Mobile WiMAX following WiMAX Forum Mobile System Profile Revision-1.4.0. In UL, when each user has only one transmit antenna, two users can transmit collaboratively in the same slot as if two streams are spatially multiplexed from two antennas of the same user. This is called UL collaborative SM.
|
Supported STC/MIMO/SISO Mode for DL-PUSC |
Parameter Settings |
|||||||
|---|---|---|---|---|---|---|---|---|
|
(In System Configuration Wizard) |
||||||||
|
Simulate Transmitter Antenna Signals |
2-antenna |
2 |
- |
Multiple Antennae |
Two Instruments |
Off |
Matrix A |
Downlink Only (TDD) or Downlink Only (FDD) |
|
2-antenna |
2 |
2 |
Multiple Antennae |
Two Instruments |
Off |
Matrix B |
Downlink Only (TDD) or Downlink Only (FDD) |
|
|
SISO |
1 |
1 |
Single Antenna |
One Instruments |
Off |
None |
Downlink Only (TDD) or Downlink Only (FDD) |
|
|
Simulate Receiver Antenna Signals |
STC (Matrix A), one-antenna
|
2 |
1 |
Single Antenna |
One Instruments |
On |
Matrix A |
Downlink Only (TDD) or Downlink Only (FDD) |
|
STC (Matrix A), 2-antenna
|
2 |
2 |
Multiple Antennae |
Two Instruments |
On |
Matrix A |
Downlink Only (TDD) or Downlink Only (FDD) |
|
|
MIMO (Matrix B), 2-antenna
|
2 |
2 |
Multiple Antennae |
Two Instruments |
On |
Matrix B |
Downlink Only (TDD) or Downlink Only (FDD) |
|
|
SISO
|
1 |
1 |
Single Antenna |
One Instruments |
On |
None |
Downlink Only (TDD) or Downlink Only (FDD) |
|
|
Supported Collaborative SM/SISO Mode for Uplink |
Parameter Settings |
|||||||
|---|---|---|---|---|---|---|---|---|
|
(In System Configuration Wizard) |
||||||||
|
Simulate Transmitter Antenna Signals |
Collaborative SM 1x2 to simulate the antenna on one of the MS |
1 |
2 |
Single Antenna |
One Instruments |
Off |
Added in PUSC Zone |
Uplink Only (TDD) or Uplink Only (FDD) |
|
Collaborative SM 1x2 to simulate both antennas of the two MS1 |
1 |
2 |
Multiple Antennae |
Two Instruments |
Off |
Added in PUSC Zone |
Uplink Only (TDD) or Uplink Only (FDD) |
|
|
SISO |
1 |
1 |
Single Antenna |
One Instruments |
Off |
None |
Uplink Only (TDD) or Uplink Only (FDD) |
|
|
Simulate Receiver Antenna Signals |
UL Collaborative 1x2 SM2
|
1 |
2 |
Multiple Antennae |
Two Instruments |
On |
Added in PUSC Zone |
Uplink Only (TDD) or Uplink Only (FDD) |
|
SISO
|
1 |
1 |
Single Antenna |
One Instruments |
On |
None |
Uplink Only (TDD) or Uplink Only (FDD) |
|
1. When fading is not turned on, this software creates waveforms that correspond to the transmitted signals from the two subscriber stations. The master instrument will have the signal from the first subscriber with pilot pattern A, while the slave source will have the signal from the second subscriber with pilot pattern B. In this case, you can not combine regular data bursts with the collaborative SM burst, because those would be coming from other subscribers.
2. When fading is enabled, this software generates the waveforms that would be received by the two base station antennae. In this scenario, you can include both regular bursts and the collaborative bursts. Two sets of fading channel parameters can be specified, each representing the conditions between one of the subscriber stations and the two base station antenna in a 1x2 SM configuration. The first set of channel parameters are applied to any regular bursts.