Go to topic Go to description Go to description Go to description Go to description Go to description Go to description Go to topic Go to topic Go to topic Go to topic

2. Basic

2. Basic: Baseband Channel Assignment (PXB)

Frequency

Range: for specified range values, see the signal generator's data sheet

Set or change the signal generator's carrier frequency. The default values are specific to the system configuration:

The signal generator output frequency is:

Signal Generator Output Frequency = Frequency – Frequency Offset

Minimum Frequency = 100 kHz + Frequency Offset

Maximum Frequency = SigGen Max + Frequency Offset

Frequency Offset

Range: –200 to 200 GHz

Set or change the frequency range limits and the visual display on the signal generator. It allows the source frequency display to account for a system with frequency translation in it.

The actual output frequency and frequency range limits for the signal generator are offset by the frequency offset value.

Signal Generator Output Frequency = Frequency – Frequency Offset

Minimum Frequency = 100 kHz + Frequency Offset

Maximum Frequency = Signal Generator Max + Frequency Offset

Amplitude

Range:

MXG: –144 to 17 dBm

ESG: –136 to 30 dBm

PSG: –130 to 30 dBm

Set or change the signal generator output amplitude.

The actual output amplitude and amplitude range limits are offset by the amplitude offset:    

Signal Generator Output Amplitude = Amplitude – Amplitude Offset

Minimum Amplitude = Signal Generator Minimum + Amplitude Offset

Maximum Amplitude = Signal Generator Maximum + Amplitude Offset     

It is not possible to set the maximum amplitude level with the ALC set to On.   

PSG Maximum = 30 dBm, Maximum with ALC Enable = On, 25 dBm

ESG Maximum = 25 dBm, Maximum with ALC Enable = On, 20 dBm     

When Attenuator Hold is Off, setting the amplitude also sets the ALC level and the attenuator. The ALC level and attenuator value are chosen to keep the ALC level at its optimum level.

When the Attenuator Hold is On, the attenuator value is held constant. Changing the amplitude or ALC level causes the other parameter to change an equal amount. In general, ignoring amplitude offset, the output amplitude is:             

Amplitude(dBm) = ALC Level(dBm) – Attenuator Value(dB)

Amplitude Offset

Range: –200 to 200 dB

Set or change an offset to the value and range limits of the signal generator amplitude.

If there is an amplifier with 10 dB of gain on the output of the signal generator, the amplitude offset should be set to 10 dB. Now all entries to the amplitude value account for this external gain.

The actual output amplitude of the signal generator is:

Signal Generator Output Amplitude = Amplitude – Amplitude Offset

Baseband Channel Assignment (PXB)

Range: 1 to 16

Default: 1

When you establish a connection between the Signal Studio software and the PXB, Signal Studio recognizes the number of baseband generators (BBGs) in the currently loaded PXB configuration. Signal Studio creates a waveform file (Ant0, Ant1, Ant2, and so on) for each antenna configured in the System Configuration Wizard. The default behavior is for Signal Studio to download waveform file Ant0 to BBG1 in the PXB, waveform file Ant1 to BBG2, and so on. In the Baseband Channel Assignment cell, the default BBG assignments are displayed as a comma-separated list (1,2).  

The Baseband Channel Assignment parameter enables you control the assignment of each waveform file to a specific BBG resource, rather than accepting the default. You can assign Ant0 to BBG2 and Ant1 to BBG1 by making the corresponding change to the comma separated list (2,1).

RF Output

Double-click or use the drop-down menu to control the operating state of the RF signal.

Mod Output

Double-click or use the drop-down menu to turn the signal generator RF modulation on or off. This function turns on or off all enabled modulation formats including I/Q modulation, pulse modulation, AM, FM, and so on.

1. Configuration

2. Basic

3. I/Q

4. ALC

5. DualARB

6. DualARB Marker Utilities

7. Dual ARB Trigger

Hardware

Waveform Setup