Double-click or use the drop-down menu to set the active polarity of the selected marker to either positive or negative. The default value is positive.
Double-click or use the drop-down menu to select a marker for this function. When the marker signal is high and the marker polarity is positive, the waveform is blanked until an enabled marker is encountered. When the marker polarity is negative, the waveform is blanked when it encounters an enabled marker. Selecting disconnects all markers from pulse routing. Details...
Double-click or use the drop-down menu to select a marker for this function. When the specified marker signal is low, ALC Hold is enabled. With ALC Hold enabled, the output power leveling does not respond to changes to the signal amplitude. Selecting disconnects all markers from ALC Hold. Details...
Double-click or use the drop-down menu to select a marker for the alternate amplitude function. When the marker signal is low, the alternate amplitude settings configured on the ESG signal generator are active. Selecting disconnects all markers from the alternate amplitude function.
This parameter is not available with all instrument model numbers and may be grayed out.
6. DualARB Marker Utilities