Last updated: January 15, 2009
The UE uses open loop power control to determine the transmit power of the first PRACH preamble and of the DPCH as it is first turned on. Once the DPCH is established its power is controlled solely by closed loop power control (see Uplink Closed Loop Power Control Parameters and UE Target Power ).
The test set calculates the expected transmit power of the first PRACH preamble and of the DPCH (at turn-on the DPCH consists only of the DPCCH) and displays them in the
UE Expected Open Loop Transmit Power
window on the
Call Setup Screen
.
The test set calculates the expected transmit power of the first PRACH preamble using the following formula (see 3GPP TS 25.331 8.5.7):
Initial PRACH TX Power = Primary CPICH TX power - CPICH RSCP + Uplink Interference + Constant value
Three parameters are directly user-settable: Primary CPICH TX Power , Uplink Interference , and Constant Value .
The fourth parameter,
CPICH RSCP (Received Signal Code Power)
, is the result of the UE reported measurement of the CPICH code channel power. You can change the test set's CPICH code channel power by varying
Cell Power
and/or
CPICH Level
(see
Downlink Channel Levels
and
CALL:STATus:CPIChannel[:CELL[1]]:POWer[:AMPLitude]?
).
GPIB command: CALL:UPLink:PRAChannel:POWer:INITial?
Per 3GPP TS 25.331 s8.5.3, the UE determines its initial DPCCH transmit power using the following formula:
DPCCH_Initial_power = DPCCH_Power_offset - CPICH_RSCP
The UE determines "CPICH_RSCP" by measuring the test set's CPICH code channel power. "DPCCH_Power_offset" is signalled by the test set in the RRC Connection Setup and Radio Bearer Setup messages used to establish the connection. The test set signals a value for DPCCH_Power_offset that places the UE's initial transmission near the
UE Target Power
setting (because the test set's receiver is ranged based on the
UE Target Power
setting). Thus, to determine what DPCCH_Power_offset value to signal during call establishment, the test set considers the
UE Target Power
setting, as well as the
Cell Power
and
CPICH Level
settings (which determine the CPICH RSCP the UE will measure).
As mentioned above, the test set signals a value for DPCCH_Power_offset that places the UE's initial transmission
near
the
UE Target Power
setting. The UE's initial transmission consists only of the DPCCH. The
UE Target Power
setting is the level you wish for the UE's DPCCH+DPDCH transmission. Thus, the test set places the initial transmit power of the UE's DPCCH slightly lower than the
UE Target Power
setting so that when the DPDCH is turned on, the total UE power matches the
UE Target Power
setting. The initial DPCCH power can thus be determined by the following formula:
Initial DPCCH TX Power = UE Target Power + 10 log (Beta c ^2/(Beta c ^2 + Beta d ^2))
All three parameters are user settable, see UE Target Power and Uplink DPCH Bc/Bd Control .
As an example, when
Cell Power
= -75 dBm,
CPICH Level
= -3.3 dB,
UE Target Power
= -5 dBm, Betac = 8/15 and Betad = 15/15, the value signalled for DPCCH_Power_offset is -44 (-88 dB) so that the
Initial DPCCH TX Power
is near -11.55 dBm (note that the actual level achieved is within 2 dB due to the fact that the information element's range is specified in steps of 2).
GPIB command: CALL:UPLink:DPCChannel:POWer:INITial?
How Do I Change UE TX Power Levels?
How Do I Change Cell Parameters?
Uplink Closed Loop Power Control Parameters and UE Target Power