:DISPlay:ETUNing:COUNt
Instrument:
N1000A
DCA-M
Meas. mode:
Eye
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:DISPlay:ETUNing:COUNt <maximum_samples>
<maximum_samples> is an int.
Query Syntax
:DISPlay:ETUNing:COUNt?
Description
Sets the decay of the persistence shown with eye tuning. Eye tuning works by weighting recent waveforms more heavily than older waveforms in the eye diagram database. The integer argument specifies exactly how many samples you want to keep in the eye diagram. For example, if you specify 50,000 samples and once there are 50,000 samples in the eye, then one sample will drop out of the eye for every new sample placed in the eye. Use the :DISPlay:ETUNing command to turn eye tuning on or off.