:EMODules:CRECovery:SADDress
Command:
Deprecated
Instrument:
N4877A
Support:
Obsolete
Deprecated command. FlexDCA A.07.90 and above not longer supports the Keysight N4877A Clock/Data Recovery and Demultiplexer.
Command Syntax
:EMODules:CRECoveryN:SADDress <SICL address>
Where N identifies slot number {1:8} which is associated with clock recovery module. On 86108A modules, specify slot 1.
<SICL address> is a string.
Query Syntax
:EMODules:CRECoveryN:SADDress?
Description
Specifies the SICL address of an extended module. To specify a VISA address, use the :CRECovery:VADDress command. Use the :SLOT:ADDRess command to select the type of address. Use the :SLOT:CONNect command to actually establish the LAN connection.
Requires FlexDCA revision A.02.00 through A.07.81.