:GRAPh:GDELay:Y:OFFSet
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
TDR
Flex Apps:
FlexDCA
Command Syntax
:GRAPh:GDELay{1:4}:Y:OFFSet <seconds>
Where the <seconds> is a double.
Where the {1:4} specifier identifies one of four waveform content windows.
Query Syntax
:GRAPh:GDELay{1:4}:Y:SCALe?
Description
Sets the vertical offset of the specified GrpDelay (group delay) content window in seconds at the Y-axis's center graticule. Use the :AUToscale sibling command to automatically set the offset and scale settings. Use the :AUToscale parent command to automatically scale both the waveform in both X and Y axis.
Requires FlexDCA revision A.03.00 and above.