:GRAPh:MAGNitude:X:STOP
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
TDR
Flex Apps:
FlexDCA
Command Syntax
:GRAPh:MAGNitude{1:4}:X:STOP <frequency>
Where the <frequency> is a double.
Where the {1:4} specifier identifies one of four waveform content windows.
Query Syntax
:GRAPh:MAGNitude{1:4}:X:STOP?
Description
For the specified Freq-Mag waveform content window, sets the graph's X- axis stop frequency in Hertz. Use the :AUToscale sibling command to automatically set the center, span, start, and stop settings. Use the :AUToscale parent command to automatically scale both the waveform in both X and Y axis.
Requires FlexDCA revision A.03.00 and above.