:GRAPh:PHASe:X:AUToscale
Instrument:
DCA-X
DCA-M
Meas. mode:
Scope
Eye
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:GRAPh:PHASeN:X:AUToscale
Where N specifies one of four {1:4} waveform content windows.
Description
Automatically scales the X-axis of the specified Phasewaveform content window. Use the :CENTer, :SPAN, :STARt, and :STOP sibling commands to individually set these values.
Requires FlexDCA revision A.03.00 and above.