:LTESt:LLINe:SSUMmary:STATe
Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:LTESt:LLINe:SSUMmary:STATe {ON | OFF}
Query Syntax
:LTESt:LLINe:SSUMmary:STATe?
Description
Turns on or off the reporting action to save an ASCII summary file whenever a limit testing for a limit line test stops data acquisition. The file name extension of summary files is .sum. Use the :LTESt:LLINe:SSUMary:FNAMe command to specify the name of the summary file. To turn on or off testing limits for a specified limit line test, use the :LTESt:LLINe:TEST:STATe command.
Requires FlexDCA revision A.04.50 and above.
Example Summary File
Limit Line Limit Test Summary
02/10/2015 13:54:52
Test Name : Upper Limit
Source : Channel 1A
Test Result: FAIL
Test Margin: -5.52 mV (at 603.50 ps)
Line Name Type Margin Location Result
====== ==================== ==== ================ ================ ======
0 Upper Rail MAX -5.52 mV 603.50 ps FAIL
Example
// Load and start limit line test. :LLINe1:LOAD:FNAMe "%USER_DATA_DIR%\Limit Lines\Golden Test.lltx" :LLINe1:SOURce CHANnel1A :LLINe1:DISPlay ON :ACQuire:STOP :ACQuire:CDISplay // Configure "Save Summary" reporting. :LTESt:LLINe:SSUMmary:FNAMe "%USER_DATA_DIR%\Limit Summaries\MyLimitTest.sum" // Enter file name. :LTESt:LLINe:SSUMmary:STATe ON // Enable summary report save.// Run limit testing. :LTESt:LLINe:TEST1:MODe SOFailure // Stop limit testing on fail condition. :LTESt:LLINe:TEST1:STATe ON // Enable limit testing. :ACQuire:RUN // Enable data acquisition.
Example Command
:LTESt:LLINe:SSUMmary:STATe ON