:LTESt:LLINe:TEST:MODe
Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:LTESt:LLINe:TEST{1:64}:MODe {SOFailure | SOSuccess}
Where {1:64} identifies the specific limit line test.
Query Syntax
:LTESt:LLINe:TEST{1:64}:MODe?
Description
Specifies the event that stops data acquisition when testing limits for a limit line test are enabled. To enable testing limits, use the :LTESt:LLINe:TEST:STATe command.
| Argument | Description |
|---|---|
| SOFailure | Stop data acquisition when the first failed data point occurs. |
| SOSuccess | Stop data acquisition when the first passing data point occurs. |
Requires FlexDCA revision A.04.50 and above.
Example Command
:LTESt:LLINe:TEST2:MODe SOFailure