Mask Tests

Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT

Creating a Eye Mask Limit Test

The following example shows how to create a limit test on eye mask number 3 and run the test until 100 failures have occurred. After the test completes, results are reported:

  • Waveform is saved to a file.
  • Summary file is created.
  • Monochrome screen image of the entire FlexDCA display is saved to a JPG file.

You can create a test for each active eye mask.

:ACQuire:SINGle
:LTESt:MTESt:MRESult3:FAILures 100
:LTESt:MTESt:SWAVeform:CHAN1A:STATe DISK
:LTESt:MTESt:SWAVeform:CHAN1A:FNAMe "C:\Users\kentb\Documents\Keysight\FlexDCA\Waveforms\Mask Waveform.wfmx"
:LTESt:MTESt:SSUMmary:STATe ON
:LTESt:MTESt:SSUMmary:FNAMe "C:\Users\kentb\Documents\Keysight\FlexDCA\Limit Summaries\Mask Test 1.sum"
:LTESt:MTESt:SIMage:STATe ON
:LTESt:MTESt:SIMage:MONochrome ON
:LTESt:MTESt:SIMage:WINDow DISPlay
:LTESt:MTESt:SIMage:FNAMe "C:\Users\kentb\Documents\Keysight\FlexDCA\Screen Images\Mask.jpg"
:LTESt:MTESt:MRESult1:STATe ON
:ACQuire:RUN
*OPC?