:MEASure:AMPLitude:DI:LEVel
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Amplitude
Command Syntax
:AMPLitude:DI:LEVel.htm {LEVel3 | LEVel2 | LEVel1 | LEVel0}
Description
Selects the logic level at which to perform the DI measurement. For NRZ signals, selects level 0 or 1. For PAM4 signals, selects level 0, 1, 2, or 3.
NRZ Waveform
PAM4 Waveform
Query Response
{LEVel3 | LEVel2 | LEVel1 | LEVel0}
Requires FlexDCA revision A.05.60 and above.