:MEASure:AMPLitude:Q:EYE
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Amplitude
Command Syntax
:MEASure:AMPLitude:Q:EYE {EYE0 | EYE1 | EYE2}
Query Syntax
:MEASure:AMPLitude:Q:EYE?
Description
This command allows you to select an eye on PAM4 signals for the :MEASure:AMPLitude:Q measurement. For NRZ signals, the argument EYE0 is automatically selected and cannot be changed. The query form of the command returns the currently selected eye.
Requires FlexDCA revision A.05.60 and above.