:MEASure:AMPLitude:SERLimit:EYE
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Amplitude
Command Syntax
:MEASure:AMPLitude:SERLimit:EYE {EYE0 | EYE1 | EYE2}
Query Syntax
:MEASure:AMPLitude:SERLimit:EYE?
Description
This command allows you to select an eye on PAM4 signals. For NRZ signals, the argument EYE0 is automatically selected and cannot be changed. The command selects the PAM4 eye on which to perform the :SERLimit measurement. The query form of the command returns the currently selected eye.
Requires FlexDCA revision A.05.60 and above.