:MEASure:AMPLitude:UN:STATus:DETails?
Query Syntax
:MEASure:AMPLitude:UN:STATus:DETails?
Description
Returns a string that may provide additional details for a failed :AMPLitude:UN measurement. If the measurement was successful, a null string is returned.
For a basic description of a measurement failure, use the :STATus:REASon? sibling query. Use the :STATus? parent query to determine if the measurement has failed.
Requires FlexDCA revision A.05.60 and above.
Measurement Identification
Avoid subtle programming errors! To ensure that the correct measurement is installed or queried, always explicitly identify a measurement when installing a measurement or querying a measured value, status, or detail. To identify a measurement, specify the measurement's source waveform (:SOURce child command). With some measurements, you may also need to specify other identifying values. Generally, when selecting a measurement using FlexDCA's GUI, if a dialog appears prompting you to select values, you should explicitly specify these values when remotely identifying the measurement. More information.
For example, to return the status of the measurement, :MEASure:AMPLitude:UN
flex.write(':MEASure:AMPLitude:UN:SOURce CHAN1A')
if flex.query(':MEASure:AMPLitude:UN:STATus?') == 'CORR';
measurement = flex.query(':MEASure:AMPLitude:UN?')
else:
details = flex.query(':MEASure:AMPLitude:UN:STATus:DETails?')
reason = flex.query(':MEASure:AMPLitude:UN:STATus:REASon?')