:MEASure:AMPLitude:VECLosure:EYE
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Amplitude
Command Syntax
:MEASure:AMPLitude:VECLosure:EYE {EYE0}
Query Syntax
:MEASure:AMPLitude:VECLosure:EYE?
Query Response
{EYE0}
Description
This command allows you to select an eye on PAM4 signals. For NRZ signals, the 0 eye is automatically selected and cannot be changed. The command selects the PAM4 eye on which to perform the :MEASure:AMPLitude:VECLosure. The query form of the command returns the currently selected eye.
unknown
Requires FlexDCA revision A.06.60 and above.