:MEASure:EYE:DI:LEVel

Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
NRZ
PAM4/6/8

Command Syntax

:MEASure:EYE:DI:LEVel {LEVel0 | LEVel1 | LEVel2 | LEVel3}

Query Syntax

:MEASure:EYE:DI:LEVel?

Description

Selects the eye diagram's level on which to perform the DI measurement. The LEVel2 and LEVel3 arguments apply only to PAM4 signals. If you experience difficulties measuring a PAM4 signal, confirm that the signal-type setting is set to PAM4 with the :CHANnel:SIGNal:TYPE command.

NRZ Waveform
PAM4 Waveform

Requires Option 401, Advanced Eye Analysis Software license.

Requires FlexDCA revision A.05.30 and above.