:MEASure:EYE:PAM:ESKew:EYE

Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
NRZ
PAM4/6/8

Command Syntax

:MEASure:EYE:PAM:ESKew:EYE EYE{0:6}

Query Syntax

:MEASure:EYE:PAM:ESKew:EYE?

Description

This command allows you to select an eye on PAM4/6/8 signals on which to perform the :MEASure:EYE:PAM:ESKew measurement. For NRZ signals, the argument EYE0 is automatically selected and cannot be changed. If you experience difficulties measuring a PAM4 signal, confirm that the signal-type setting is set to PAM4, PAM6, or PAM8 with the :CHANnel:SIGNal:TYPE command.

NRZ Waveform
PAM4 Waveform
PAM6 Waveform
PAM8 Waveform

Requires FlexDCA revision A.04.50 and above.