:MEASure:EYE:PAM:LINearity:DEFinition

Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
PAM4/6/8

Command Syntax

:MEASure:EYE:PAM:LINearity:DEFinition {RLMA120 | RLMC94 | EYE}

Query Syntax

:MEASure:EYE:PAM:LINearity:DEFinition?

Query Response

 {RLMA120 | RLMC94 | EYE}

Description

Selects the algorithm used to measure RML (Ratio Level Mismatch) linearity on a PAM signal in Eye mode. The definition arguments are listed in the following table.

Linearity Measurement Definitions
Available Measurement Definitions :MEAS:EYE:PAM:LIN:DEF
SCPI Command Argument
Compatible Waveforms
NRZ PAM4 PAM6 PAM8
RLM (Ratio Level Mismatch) (IEEE 802.3 Annex 120D). RLMA120 ● ●
RLM (Ratio Level Mismatch) (IEEE 802.3 Clause 94). This is the default setting. RLMC94 ● ● ● ●
Eye Linearity (CEI 4.0) EYE ● ● ● ●

Requires FlexDCA revision A.05.70 and above.