:MEASure:EYE:PEECq:STATus:DETails?
Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
PAM4
Query Syntax
:MEASure:EYE:PEECq:STATus:DETails?
Description
Returns a string that may provide additional details for a failed :MEASure:EYE:PEECq? measurement. If the measurement was successful, a null string is returned. Use the :MEASure:EYE:PEECq:STATus? query to determine if the measurement has failed. Use the :MEASure:EYE:PEECq:STATus:REASon? query the reason that a measurement has failed.
Requires FlexDCA revision A.07.90 and above.
Example Command
:MEASure:EYE:PEECq:STATus:DETails?