:MEASure:EYE:PTDeq:SOURce

Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
PAM4

Command Syntax

:MEASure:EYE:PTDeq:SOURce <source_waveform>

Where <source_waveform> can be one of the following:

  • CHANnel{1:8}{A|B|C|D}
  • DIFF{1:4}
  • CGMemory{1:8}
  • FUNCtion{1:16}

Query Syntax

:MEASure:EYE:PTDeq:SOURce?

Query Response

<source_waveform>

Description

Selects the source waveform on which to perform a Partial TDECQ measurement (:MEASure:EYE:PTDeq).

Requires FlexDCA revision A.05.70 and above.