:MEASure:EYE:TI:TIBer
Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
NRZ
PAM4/6/8
Command Syntax
:MEASure:EYE:TI:TIBer <BER>
<BER> is a double.
Query Syntax
:MEASure:EYE:TI:TIBer?
Description
Sets the BER level at which to perform the Total Interference (TI) measurement. By default the measurement is made at a BER of 1E-12 (1 x 10–12), which is a probability of occurrence of less than 1 part per trillion. The BER can be set to any value between 1E-1 to 1E-18.
Requires FlexDCA revision A.05.30 and above.