:MEASure:HISTogram:PPOSition:STATus?
Meas. mode:
Eye
Scope
TDR
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:MEASure:HISTogram{1:4}:PPOSition:STATus?
Query Response
{CORR | INV | QUES}
- CORR
- The measurement result is correct.
- INV
- The measurement result is invalid. A question mark (?) is shown in the displayed results table instead of a measurement result.
- QUES
- The measurement result is questionable. A question mark (?) is shown in the displayed results table next to the measurement result.
Description
Queries the status of the PPOSition measurement. Use the :STATus:REASon? child query to determine the reason for an invalid or questionable measurement. Additional information about the failure may be available using the :STATus:DETails? child query.