:MEASure:JITTer:DDJ:EYE

Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Jitter

Command Syntax

:MEASure:JITTer:DDJ:EYE {EYE0 | EYE1 | EYE2}

Query Syntax

:MEASure:JITTer:DDJ:EYE?

Description

This command selects the eye on which to perform the :DDJ measurement. For NRZ signals, the argument EYE0 is automatically selected and cannot be changed. The query form of the command returns the currently selected eye.

NRZ Waveform

This measurement can be made on PAM4 waveforms. With PAM4 waveforms, Eye 0, Eye 1, or Eye 2 can be specified.

PAM4 Waveform

Requires FlexDCA revision A.05.60 and above.