:MEASure:JITTer:EWIDth:EYE

Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Jitter

Command Syntax

:MEASure:JITTer:EWIDth:EYE {EYE0 | EYE1 | EYE2}

Query Syntax

:MEASure:JITTer:EWIDth:EYE?

Description

This command selects the eye on which to perform the :EWIDth measurement. The query form of the command returns the currently selected eye. The results are placed in the following results table:

  • Jitter table for NRZ signals.
  • Eye table for PAM4 signals.

NRZ Waveform

This measurement can be made on PAM4 waveforms. With PAM4 waveforms, Eye 0, Eye 1, or Eye 2 can be specified.

PAM4 Waveform

This is a command for PAM4 signals only. For NRZ signals, this command results in an "−221, Settings conflict " error.

Requires FlexDCA revision A.05.60 and above.