:MEASure:JITTer:POJitter:EOJ:LOCation?

Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
PAM4
Meas. panel:
Timing Jitter
Timing Jitter

Query Syntax

:MEASure:JITTer:POJitter:EOJ:LOCation?

Query Response

"<row location>"

For example, 2.

Description

Returns an index string that identifies the measurement cell of the :MEASure:JITTer:POJitter:EOJ measurement results in the Timing Jitter panel. If the measurement is not listed in the table, a "−1" is returned.

Requires FlexDCA revision A.08.30 and above.