:MEASure:JITTer:RJ:EYE
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Jitter
Command Syntax
:MEASure:JITTer:RJ:EYE {EYE0 | EYE1 | EYE2}
Query Syntax
:MEASure:JITTer:RJ:EYE?
Description
This command selects the eye on which to perform the :RJ measurement. For NRZ signals, the argument EYE0 is automatically selected and cannot be changed. The query form of the command returns the currently selected eye.
NRZ Waveform
This measurement can be made on PAM4 waveforms. With PAM4 waveforms, Eye 0, Eye 1, or Eye 2 can be specified.
PAM4 Waveform
Requires FlexDCA revision A.05.60 and above.