:MEASure:MTESt:HRatio:STATus:DETails?
Meas. mode:
Eye
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:MEASure:MTEStN:HRatio:STATus:DETails?
Description
Returns a string that may provide additional details for a failed :MTESt:HRatio measurement. If the measurement was successful, a null string is returned.
For a basic description of a measurement failure, use the :STATus:REASon? sibling query. Use the :STATus? parent query to determine if the measurement has failed.