:MEASure:MTESt:MUNCertainty:STATus?
Meas. mode:
Eye
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:MEASure:MTESt{N}:MUNCertainty:STATus?
{N} identifies a specific mask and must be a value from 1 to 16. For example, :MTESt2: selects mask 2.
Query Response
{CORR | INV | QUES}
- CORR
- The measurement result is correct.
- INV
- The measurement result is invalid. A question mark (?) is shown in the displayed results table instead of a measurement result.
- QUES
- The measurement result is questionable. A question mark (?) is shown in the displayed results table next to the measurement result.
Description
Queries the status of the MUNCertainty measurement. Use the :STATus:REASon? child query to determine the reason for an invalid or questionable measurement. Additional information about the failure may be available using the :STATus:DETails? child query.