:MEASure:OSCilloscope:JITTer:FORMat
Flex Apps:
FlexDCA
Meas. mode:
Scope
Waveform type:
NRZ
PAM4/6/8
Command Syntax
:MEASure:OSCilloscope:JITTer:FORMat {PP | RMS}
Description
Select the format for oscilloscope-mode jitter measurement: JitterRMS or JitterPP (peak-to-peak). Use the :MEASure:OSCilloscope:JITTer command to perform the measurement.
Example Command Sequence
:SYSTem:MODE OSCilloscope :MEASure:OSCilloscope:JITTer:SOURce CHAN1A :MEASure:OSCilloscope:JITTer:DJFormat PP :MEASure:OSCilloscope:JITTer :MEASure:OSCilloscope:JITTer?