:MEASure:PEYE:EHEight:EYE
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
PAM4
Meas. panel:
Eye
Command Syntax
:MEASure:PEYE:EHEight:EYE {EYE0 | EYE1 | EYE2}
Query Syntax
:MEASure:PEYE:EHEight:EYE?
Description
This command selects the PAM4 eye on which to perform the :EHEight measurement. The query form of the command returns the currently selected eye.
This is a command for PAM4 signals only. For NRZ signals, this command results in an "−221, Settings conflict " error.
Requires FlexDCA revision A.06.00 and above.