:MEASure:PEYE:PJRMs:STATus?

Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
PAM4
Meas. panel:
Eye

Query Syntax

:MEASure:PEYE:PJRMs:STATus?

Query Response

{CORR | INV | QUES}
CORR
The measurement result is correct.
INV
The measurement result is invalid. A question mark (?) is shown in the displayed results table instead of a measurement result.
QUES
The measurement result is questionable. A question mark (?) is shown in the displayed results table next to the measurement result.

Description

Queries the status of the PJRMs measurement. Use the :STATus:REASon? child query to determine the reason for an invalid or questionable measurement. Additional information about the failure may be available using the :STATus:DETails? child query.

Measurement Identification

Avoid subtle programming errors! To ensure that the correct measurement is installed or queried, always explicitly identify a measurement when installing a measurement or querying a measured value, status, or detail. To identify a measurement, specify the measurement's source waveform (:SOURce child command). With some measurements, you may also need to specify other identifying values. Generally, when selecting a measurement using FlexDCA's GUI, if a dialog appears prompting you to select values, you should explicitly specify these values when remotely identifying the measurement. More information.

For example, to return the status of the measurement, :MEASure:PEYE:PJRMs

flex.write(':MEASure:PEYE:PJRMs:SOURce CHAN1A')
if flex.query(':MEASure:PEYE:PJRMs:STATus?') == 'CORR';
    measurement = flex.query(':MEASure:PEYE:PJRMs?')
else:
	details = flex.query(':MEASure:PEYE:PJRMs:STATus:DETails?')
	reason = flex.query(':MEASure:PEYE:PJRMs:STATus:REASon?')