:MEASure:PEYE:RJ:SOURce
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
PAM4
Meas. panel:
Eye
Command Syntax
Only use the query form of this command. Refer to the description below for more information.
Query Syntax
:MEASure:PEYE:RJ:SOURce?
Description
Because Jitter mode can only have one source waveform, there is no selection to make by sending :SOURce. However, you can use the :SOURce? query to identify the source waveform on which the RJ measurement is performed. If you want to change Jitter mode's source waveform, send one of the following commands:
:CHANnel{1A:8D}:DISPlay ON
:DIFF{1A:8C}:DISPlay ON
:FUNCtion{1:16}:DISPlay ON
:JMEMory1:DISPlay ON
You must follow the command with an autoscale as shown in the following example:
:CHANnel2B:DISPlay ON :SYSTem:AUToscale :*OPC?
Requires FlexDCA revision A.02.50 and above.