:MEASure:PEYE:TJ:EYE

Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
PAM4
Meas. panel:
Eye

Command Syntax

:MEASure:PEYE:TJ:EYE {EYE0 | EYE1 | EYE2}

Query Syntax

:MEASure:PEYE:TJ:EYE?

Description

This command selects the eye on which to perform the :TJ measurement. For NRZ signals, the argument EYE0 is automatically selected and cannot be changed. The query form of the command returns the currently selected eye.

PAM4 Waveform

Requires FlexDCA revision A.06.00 and above.