:MEASure:PEYE:UJ:EYE
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
PAM4
Meas. panel:
Eye
Command Syntax
:MEASure:PEYE:UJ:EYE {EYE0 | EYE1 | EYE2}
Query Syntax
:MEASure:PEYE:UJ:EYE?
Description
This command selects the eye on which to perform the :UJ measurement. For NRZ signals, the argument EYE0 is automatically selected and cannot be changed. The query form of the command returns the currently selected eye.
Requires FlexDCA revision A.06.00 and above.