:MEASure:PLEVel:HSYMbol:LEVel
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
PAM4
Meas. panel:
Level
Command Syntax
:MEASure:PLEVel:HSYMbol:LEVel {LEVel3 | LEVel2 | LEVel1 | LEVel0}
Description
Selects the logic level at which to perform the HSYMbol measurement. Select either LEVel0, LEVel1, LEVel2, or LEVel3.
PAM4 Waveform
Query Response
{LEVel3 | LEVel2 | LEVel1 | LEVel0}
Requires FlexDCA revision A.06.00 and above.