:MEASure:PLEVel:PIR:LEVel

Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
PAM4
Meas. panel:
Level

Command Syntax

:PLEVel:PIR:LEVel.htm {LEVel3 | LEVel2 | LEVel1 | LEVel0}

Description

Selects the logic level at which to perform the PIR measurement. Select either ZERO, ONE, TWO, or THRee.

PAM4 Waveform

Query Response

{LEVel3 | LEVel2 | LEVel1 | LEVel0}

Requires FlexDCA revision A.06.00 and above.