:MEASure:PLEVel:PI:LEVel

Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
PAM4
Meas. panel:
Level

Command Syntax

:PLEVel:PI:LEVel.htm {LEVel3 | LEVel2 | LEVel1 | LEVel0}

Description

Selects the logic level at which to perform the PI measurement. Select either LEVel0, LEVel1, LEVel2, or LEVel3.

PAM4 Waveform

Query Response

{LEVel3 | LEVel2 | LEVel1 | LEVel0}

Requires FlexDCA revision A.06.00 and above.