:MEASure:EYE:TDEQ:OMA:VALue
Meas. mode:
Eye
Package License:
L-RND
L-MFG
Waveform type:
PAM4
Waveform record:
MV
Removed command for revision A.05.80 and above. This command is no longer available.
Command Syntax
:MEASure:EYE:TDEQ:OMA:VALue <amplitude>
<amplitude> is a double.
Query Syntax
:MEASure:EYE:TDEQ:OMA:VALue?
Description
Enters the result of Oscilloscope mode's OMA measurement (:MEASure:OSCilloscope:OMAmplitude
command. This OMA value is used when measuring TDECQ with the :MEAS:EYE:TDEQ
command. In order for this value to be used in the TDECQ calculation, you must select a user-defined definition as set by the :MEAS:EYE:TDEQ:METHod
sibling command.
The query form of the command returns the user-defined OMA value.
Requires FlexDCA revision A.05.60 and above.