:MEASure:OSCilloscope:OMAmplitude
Command Syntax
:MEASure:OSCilloscope:OMAmplitude
Query Syntax
:MEASure:OSCilloscope:OMAmplitude?
Description
Performs an Optical Modulation Amplitude (OMA) measurement on NRZ waveforms. Moves the OMA measurement to the top of the Results table. Displays the measurement if it is not already shown on the table. The query form of the command returns the measured value. OMA is the measure of the difference between the optical power of an NRZ one pulse and the optical power of an NRZ zero pulse. It requires an NRZ pattern and is designed to be used with square wave made of consecutive zeros following by consecutive ones. Be sure to check any relevant standard for one and zero run requirements. If needed, you can make an OMA measurement on any pulse train (not just a square wave) as long as enough consecutive symbols (ones or zeros) are included for the signal level to settle. Sources can be any displayed waveform, waveform memory, or function. For example, CHAN1A, WMEMory1, or FUNCtion1. Use :MEASure:TBASe:METHod to change the definition of the waveform's top/base. Use :MEASure:THReshold:METHod to change the definition of the waveform's threshold.
Measurement Ready?
To confirm that the measurement is ready to read, you can query the measurement's status:
if ('CORR' in Flex.query(':MEASure:OSCilloscope:OMAmplitude:STATus?')):
measurement = Flex.query(':MEASure:OSCilloscope:OMAmplitude?')
If averaging is turned on (:ACQuire:AVERaging), you can also confirm if the measurement result is ready by comparing the number of specified averages (:ACQuire:ECOunt?) versus the number of measurement sweeps that have occurred (:MEASure:OSCilloscope:OMAmplitude:COUNt?). The technique uses the :COUNt? common measurement query. For example,
if (Flex.query(':MEASure:OSCilloscope:OMAmplitude:COUNt?') >= Flex.query(':ACQuire:ECOUNt?')):
measurement = Flex.query(':MEASure:OSCilloscope:OMAmplitude?')
You can also use an acquisition limit lest to test that a number of waveform samples, or pattern acquisitions have completed before returning a measurement. Refer to the :LTESt:ACQuire:CTYPe command.
Common Measurement Child Queries
This command supports the use of the following common measurement queries: :LOCation?, :COUNt?, :MAXimum?, :MINimum?, :MEAN?, and :SDEViation?.
Measurement Identification
Avoid subtle programming errors! To ensure that the correct measurement is installed or queried, always explicitly identify a measurement when installing a measurement or querying a measured value, status, or detail. To identify a measurement, specify the measurement's source waveform (:SOURce child command). With some measurements, you may also need to specify other identifying values. Generally, when selecting a measurement using FlexDCA's GUI, if a dialog appears prompting you to select values, you should explicitly specify these values when remotely identifying the measurement. More information.
For example, to return the status of the measurement, :MEASure:OSCilloscope:OMAmplitude
flex.write(':MEASure:OSCilloscope:OMAmplitude:SOURce CHAN1A')
if flex.query(':MEASure:OSCilloscope:OMAmplitude:STATus?') == 'CORR';
measurement = flex.query(':MEASure:OSCilloscope:OMAmplitude?')
else:
details = flex.query(':MEASure:OSCilloscope:OMAmplitude:STATus:DETails?')
reason = flex.query(':MEASure:OSCilloscope:OMAmplitude:STATus:REASon?')
Child commands for measurement identification:
:MEASure:OSCilloscope:OMAmplitude:SOURce:MEASure:OSCilloscope:OMAmplitude:REGion
Example Command Sequence
:SYSTem:MODE OSCilloscope :MEASure:OSCilloscope:OMAmplitude:SOURce CHAN1A :MEASure:OSCilloscope:OMAmplitude :MEASure:OSCilloscope:OMAmplitude?