:MEASure:TDR:ECAPacitance:REFerence:VALue
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:MEASure:TDR:ECAPacitance:REFerence:VALue <impedance>
<impedance> is a double with units in ohms.
Query Syntax
:MEASure:TDR:ECAPacitance:REFerence:VALue?
Description
Selects the reference impedance for the excess capacitance measurement (:MEASure:TDR:ECAPacitance). The sibling command :TYPE must be set to CUSTom before the reference value can be used in the measurement.
Requires FlexDCA revision A.04.50 and above.