:MEASure:TDR:TEDGe:DIRection
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:MEASure:TDR:TEDGe:DIRection {RISing | FALLing}
Query Syntax
:MEASure:TDR:TEDGe:DIRection?
Description
For the Time-at-Edge measurement, specifies the edge direction used to identify the waveform's edge: rising or falling. To specify the edge number, use the :TDR:TEDGe:NUMBer command. To specify the edge threshold, use the :TDR:TEDGe:THReshold command.
Requires FlexDCA revision A.04.00 and above.
Example Command Sequence
:SYSTem:MODE TDR :MEASure:TDR:TEDGe:SOURce TRACe4 :MEASure:TDR:TEDGe:DIRection RISing :MEASure:TDR:TEDGe:NUMBer 2 :MEASure:TDR:TEDGe:THReshold MIDDle :MEASure:TDR:TEDGe :MEASure:TDR:TEDGe?